|    Change Country Change Location GBP
 
United Kingdom United Kingdom

Incoterms:DDP
All prices include duty and customs fees on select shipping methods.

Please confirm your currency selection:

British Pounds
Free shipping on most orders over £50 (GBP)

Euros
Free shipping on most orders over 65 € (EUR)

US Dollars
Free shipping on most orders over $100 (USD)
Home » Applications & Technologies » RF Wireless Technology
Applications & Technologies
Grant Imahara – Empowering Innovation Together
RF Wireless Technology
RF Wirelesss Diagram

A radio frequency (RF) signal refers to a wireless electromagnetic signal used as a form of communication, if one is discussing wireless electronics. Radio waves are a form of electromagnetic radiation with identified radio frequencies that range from 3Hz to 300 GHz. Frequency refers to the rate of oscillation (of the radio waves.) RF propagation occurs at the speed of light and does not need a medium like air in order to travel. RF waves occur naturally from sun flares, lightning, and from stars in space that radiate RF waves as they age. Humankind communicates with artificially created radio waves that oscillate at various chosen frequencies. RF communication is used in many industries including television broadcasting, radar systems, computer and mobile platform networks, remote control, remote metering/monitoring, and many more.

While individual radio components such as mixers, filters, and power amplifiers can be classified according to operating frequency range, they cannot be strictly categorized by wireless standard (e.g. Wi-Fi, Bluetooth, etc.) because these devices only provide physical layer (PHY) support. In contrast, RF modules, transceivers, and SoCs often include data link layer support for one or more wireless communication protocols. These products are organized by wireless technology and can be browsed under the “Solutions” tab.

Bluetooth Solutions
ZigBee Solutions
Wi-Fi Solutions
GPS Solutions
< 1 GHz
Click to view larger RF Wirelesss Diagram
Click to enlarge

Although wireless communication is often associated with the 2.4 GHz frequency range, many devices and technologies use radio frequencies below 1 GHz (1000 MHz). The 900 MHz band, or 33-centimeter band, is a well-known ISM (industrial, scientific and medical) frequency range used for cordless phones, walkie-talkies, amateur radio and even amateur television. ZigBee, a specification for low-power communication in wireless personal area networks (WPANs), as well as the IEEE 802.15.4 standard it is based on, can use the 900 MHz ISM band in the Americas.

Also in the sub- GHz range is Citizens’ Band (CB) radio, a popular two-way amateur radio service occupying the 26.79 MHz to 27.4 MHz range in the United States. Both AM broadcast radio (535 KHz – 1.7 MHz) and FM broadcast radio (87 MHz – 108 MHz) are in this lower range of frequencies as well, and over-the-air television in the U.S. spans a wide (54 MHz to 806 MHz) range of carrier frequencies. Recent near field communication technology (NFC), found today in many of the newest smartphones, operates at 13.56 MHz.

» Antennas » RF Switches » Filters » LNAs (Low Noise Amplifiers) » Power Amplifiers » Buffers » Mixers » VCOs (Voltage Controlled Oscillators)
1 GHz - 5 GHz
Click to view larger RF Wirelesss Diagram
Click to enlarge

The 2.4 GHz ISM (industrial, scientific and medical) band is perhaps the most common in this frequency range. Its unlicensed nature has made the ISM bands a popular choice for many wireless technologies, such as ZigBee (IEEE 802.15.4), Bluetooth (IEEE 802.15.1), and Wi-Fi (802.11).

Many other 2.4GHz technologies exist as well; WiMAX, GPS, cordless phones, car alarms, and even microwave ovens operate in this frequency range.

» Antennas » RF Switches » Filters » LNAs (Low Noise Amplifiers) » Power Amplifiers » Buffers » Mixers » VCOs (Voltage Controlled Oscillators)
> 5 GHz
Click to view larger RF Wirelesss Diagram
Click to enlarge

Wireless signals in the upper end of the super high frequency (SHF) band and higher (5 GHz+) are often referred to as microwaves. At these frequencies water is more or less “opaque”, so a microwave signal will experience significant attenuation and scattering issues due to moisture in the air. For this reason, extremely high frequency communications are either severely limited in range or always require line of sight.

Still, these types of signals can be made highly directional, and are seeing increasing use in modern technology. The ISM (industrial, scientific and medical) bands include several frequencies in the high GHz range such as Wi-Fi based on IEEE 802.11a and 802.11n wireless standards, which both 5 GHz capable. IEEE 802.11ac is the latest standard standard for emerging WiFi technology, operating exclusively in the 5 GHz band and offering significant improvements in speed, range, power consumption, and reliability. Other new technologies are designed to opearate on frequency bands much higher still; WirelessHD is a wireless specification based and frequencies as high as 60 GHz and features an impressive maximum nominal data rate of 25 gigabits per second – rivaling that of HDMI.

» Antennas » RF Switches » Filters » LNAs (Low Noise Amplifiers) » Power Amplifiers » Buffers » Mixers » VCOs (Voltage Controlled Oscillators)
Bluetooth
Point-to-Point Network Topology Diagram

Based on the IEEE 802.15.1 standard for wireless personal area networks (WPANs), Bluetooth technology is designed to provide reliable, low-power wireless communications over short distances.

Why choose Bluetooth?

Bluetooth is best known as the primary technology for wirelessly connecting mobile phones with peripheral devices such as wireless headsets. However, Bluetooth radios can be an ideal choice for a wide range of designs. Bluetooth may be a good fit if your product:

  • Would benefit from quick and easy wireless connectivity
  • Calls for data rates many times greater than ZigBee (IEEE 802.15.4)
  • Requires greater portability and lower power consumption than Wi-Fi (IEEE 802.11)

» Bluetooth / 802.15.1 Modules » Bluetooth / 802.15.1 Development Tools
ZigBee
Mesh Network Topology Diagram

ZigBee, like Bluetooth, is a specification for communication in wireless personal area networks (WPANs). Designed to be low cost, low power and low duty cycle, ZigBee technology is ideal for wireless sensor networks (WSNs) and other low power networks that span potentially large distances. ZigBee builds upon the IEEE 802.15.4 standard, but adds mesh networking capability with multi-hop functionality and a routing protocol. Star networks as well as peer-to-peer (e.g., mesh and cluster tree) are supported, making ZigBee networks dynamic, scalable, and decentralized.

ZigBee technology is not meant to compete with technologies such as Wi-Fi (IEEE 802.11) or Bluetooth (IEEE 802.15.1). Rather, ZigBee is designed for applications where data transfer rate is much less important than power efficiency, network size, and the capacity for ad hoc routing.

» ZigBee / 802.15.4 Modules » ZigBee / 802.15.4 Development Tools
Wi-Fi
Point-to-Multipoint Topology Diagram

Virtually all wireless local area networks (WLANs) are based upon the IEEE 802.11 standard for WLANs, called “Wi-Fi”. Nearly all of today's smartphones, laptops, tablets, and eBook readers are Wi-Fi capable – with very few exceptions. WLANs allow computer networks to be established for often a fraction of the cost of installing wired Ethernet, and can be used for temporary Wi-Fi connection “hotspots” in hotels, coffee shops, airports, libraries, and more. There are a range of standards within IEEE 802.11, each denoted by a letter suffix:

802.11b – This was the first Wi-Fi standard to be widely used for creating wireless computer networks. It operates in the unlicensed 2.4GHz ISM frequency band and supports a maximum (nominal) data rate of 11 Mbit/s. 802.11b supports two modulation techniques: complementary code keying (CCK) and direct-sequence spread spectrum (DSSS).

» WiFi / 802.11 Modules » WiFi / 802.11 Development Tools
GPS & More

While Bluetooth, ZigBee, and Wi-Fi are some of the most prominent wireless standards, there are certainly many other important wireless technologies.

The Global Positioning System (GPS) is a satellite-based global navigation system that provides accurate location and time information anywhere on the planet. GPS is an important and ubiquitous technology used in applications ranging from commercial car-based navigation to advanced military target tracking and missile guidance systems. Most GPS satellites broadcast at the same two frequencies: 1575.42MHz, called the “L1” band, and the 1227.60MHz “L2” band. The signals are encoded using a CDMA spread-spectrum technique, allowing individual satellites to be distinguished from each other without co channel interference.

Radio frequency identification (RFID) is a wireless technology analogous to UPC barcodes. It is used worldwide for tracking and identifying consumer products. RFID transponders, or tags, are placed on portable objects to be tracked or identified, whether it is vehicles, livestock, baggage, or even people. RFID readers entail greater cost and complexity, so are typically stationary – installed in locations where the RFID data exchange is to take place. RFID is used in many applications including employee access control, asset tracking, electronic toll collection, and supply chain control.

» GPS Modules » GPS Development Tools » RF Modules » RF Development Tools » RFID Transponder » RFID Transponder Tools

Texas Instruments WL18x7MOD
Dual Band Combo 2x MIMO Wi-Fi Modules

Offer high throughput and extended range along with Wi-Fi and Bluetooth coexistence (WL1837MOD only) in a power-optimized design. The WL18x7MOD is a Wi-Fi, dual-band, 2.4 and 5GHz module solution with two antennas supporting Industrial temperature grade.

Digi International XLR PRO
Long-Range 900 MHz Industrial Radio

A high performance, industrial grade long-range 900 MHz radio that offers reliable wireless communications for serial and Ethernet devices over long distances. Industry-leading range of 100+ miles and interference immunity that will punch through noisy RF environments.

Murata Type ZY
Bluetooth SMART Module

2.4GHz Bluetooth low energy module with UART/SPI interface and a DA14580 (Dialog Semiconductor) chipset. It features an internal crystal and a low 5mA of power consumption at 0dBm transmit power current in a 7.4mm x 7mm x 1mm package.

Laird Wireless
BT900 Bluetooth Modules

Laird's BT900 modules reduce the engineering burden and design risk of integrating Bluetooth and Bluetooth Low Energy into an OEM device. Its 19mm x 12.5mm form factor, optimized power schemes and smartBASIC language provide a secure, stable Bluetooth environment for any embedded design.

Lantronix xPICO WiFi Embedded
Wireless Device Servers

The most flexible, mobile-ready, Wi-Fi solution for M2M and IOT applications. These devices reduce your development costs, shorten your time to market, and leverage mobile solutions with xPico Wi-Fi, one of the world's smallest and most flexible Wi-Fi device servers.

LS Research TiWi
C-W Integrated WLAN Module

Simplifies the work of adding Wi-Fi connectivity to your products with a very small footprint. The TiWi-C-W module's breadth of capabilities ensures a straight-forward integration with your product design, including a pre-loaded cloud connectivity agent for LSR's TiWiConnect platform.
More Featured Products
Semiconductors
Analog Devices - 18GHz Microwave PLL SynthesizersLearn More
Silicon Labs - Ember® EM35x Integrated ZigBee/802.15.4 SoCLearn More
Maxim Integrated - MAX9947 AISG Integrated TransceiverLearn More
NXP Semiconductors - JN516x Wireless MicrocontrollersLearn More
Skyworks Solutions, Inc. - RF Switch ICsLearn More
TI - LMX Ultra-Low Noise Frequency SynthLearn More
TriQuint - TQP3M Series LNAsLearn More
M/A-COM Technology Solutions - RF MixersLearn More
NXP Semiconductors - BFU7XXF TransistorsLearn More
Epcos - SAW Filters and ResonatorsLearn More
Skyworks Solutions, Inc. - PA RF AmplifiersLearn More
Skyworks Solutions, Inc. - SE2595L Wireless LAN Front-EndLearn More
STMicroelectronics - SPIRIT1 Sub-1GHZ TransceiverLearn More
M/A-COM - E-Series Surface Mount RF MixersLearn More
Advanced Products
Bluegiga - BLE113 Bluetooth® Smart ModulesLearn More
TriQuint - Digital Variable Gain AmplifiersLearn More
SkyWorks - SKY65337-11 TX/RX Front-End ModulesLearn More
Modules
Microchip - RN4020 Bluetooth Low Energy ModuleLearn More
Murata - Type ZY Bluetooth SMART ModuleLearn More
Panasonic - PAN1026 Bluetooth® 4.0 ModuleLearn More
Panasonic - PAN1740 Bluetooth® Low Energy (BLE) ModuleLearn More
Taiyo Yuden - Bluetooth ModulesLearn More
Passive Components
AVX - DP Series MLO™ DiplexersLearn More
Anaren - High Frequency ResistorsLearn More
Murata - High Frequency Ceramic CapacitorsLearn More
Bourns - SRP4012 Series Power InductorsLearn More
KEMET - CBR Series RF & Microwave CapacitorsLearn More
Panasonic - ELJ-Qx Series InductorsLearn More
AVX - Multilayer Organic CapacitorsLearn More
TDK - RF ComponentsLearn More
Vishay – VJ Series High Frequency CapacitorsLearn More
Connectors
Radiall - SMP-MAX ConnectorsLearn More
Emerson Connectivity Solutions - Trompeter Twinax/Triax ConnectorsLearn More
Amphenol RF - TNC and N Rugged IP67 RF Connectors Learn More
Hirose Electric U.FL Series SMT Coaxial ConnectorLearn More
Amphenol Connex - High Performance Broadcast ConnectorsLearn More
Emerson Connectivity Solutions/Trompeter - Twinax/Triax ConnectorsLearn More
Molex - RF Connectors Learn More
Emerson Connectivity Solutions - SMA Self Fixture End Launch ConnectorsLearn More
Cable Assemblies
Molex - U.FL Cable AssembliesLearn More
Amphenol Connex - Fixed Length Cable AssembliesLearn More
Emerson Connectivity Solutions/Johnson - Fixed Length Cable AssembliesLearn More
Semflex - DKT Test Cable AssembliesLearn More
Hirose - Electric U.FL Series SMT Coaxial ConnectorLearn More

HOW TO TEST - RF WIRELESS TECHNOLOGY
Teledyne LeCroy HDO 4000 Series High Definition Oscilloscopes
Teledyne LeCroy HDO 4000 Series High Definition Oscilloscopes

Combining Teledyne LeCroy's HD4096 high definition 12-bit technology, with long memory, a compact form factor, 12.1" touch screen display and powerful debug tools, the HDO4000 is the ideal oscilloscope for precise measurements and quick debug. Pair with Lecroy ZS series active probes for high impedance across the entire system bandwidth.



 
Amplifiers
 
Antennas
 
Cellular
 
Diodes
 
General
 
GPS
 
ISM
 
LNAs
 
Oscillators
 
Reference Design
 
Regulations
 
RF Basics
 
RF Connectors
 
Amphenol
 
Avago
 
CEL
 
Crystek
 
Linx Technologies
 
MA-COM
 
Maxim Integrated
 
Murata
 
NXP
 
Silicon Labs
 
Skyworks Solutions, Inc.
 
TI